[FAQ-HW-3] Can discrete SiC MOSFET's be placed in parelell for higher currents ?
Options
SiC_Power_Admin
Wolfspeed Admin - Contributor Level 4
Yes, SiC MOSFETs can be operated in parallel much like a Si MOSFET. However, the layout is more critical due to the faster switching times on SiC devices. Maintaing symmetry in both the gate drive and power loops is one of the most important factors in good dynamic sharing.
1