[FAQ-ID-3] What are maximum ratings in a Datasheet?
TBhatia
Wolfspeed Admin - Contributor Level 5
• Typical testing condition is at 25ᵒC. The condition will be specified if it is different.
• Represent the maximum capability of the device.
• May cause damage if any of the parameter is exceeded.
• The design must guarantee no parameter is exceeded under worst case conditions.
• Always read the notes.
Tagged:
0