Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Distance between driver and module connection busbar

baiyujing
baiyujing Contributor Level 2
edited May 2023 in Module Products

Hello,

I have purchased your company's SiC module CAB450M12XM3 and its driver CGD12HBXMP. When I press and connect the driver to the module, the module pins are approximately 1cm away from the driver. But in my application, I raised the busbar connecting the module pins, and in the end, the busbar was approximately 3mm away from the driver. Can this distance ensure that the driver is not affected by high currents on the busbar?

Waiting for your reply.

Regards.

This discussion has been closed.