LTspice model question: parasitic parameters associated with discrete packages
Hi Wolfspeed experts,
According to the document, LTspice model has a parasitic component associated with the package (gate, source, drain and kelvin). When I check the parameters described in the library file (C3M0016120K.lib for this case), I found:
Ls1 and R_Ls1 : inductance & resistance of source pin & wires
Ls2 and R_Ls2 : inductance & resistance of kelvin pin & wire
Lg and R_Lg : inductance & resistance of gate pin & wire
Ld and R_Ld : inductance & resistance of drain pin & wires
Here's the question, what parameters Rv and Lv and R_gg refer to?
Thank you for your support.
Best Regards,
Hiroshi
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hi,
Lv is the inductance that is common to both the gate loop and power loop in the device. Rv and R_gg are both "convergence aides" that do not reflect device performance but are added to help the solver in LTSpice converge when running a simulation. I hope this helps!
Thanks,
Zack
0 -
Hi Zack,
I get it now. Thank you for the answer!
0