deadtime
Regarding the dead time, taking CAB450M12XM3 as an example, when the dead time of the simulation condition is set to 500ns, the dead time in summary is displayed as 0.01ns. There are similar problems under other simulation conditions, namely: The dead time of the simulation condition is not consistent with the dead time shown in the results. In this case, what is the actual dead time in the simulation process? Is it 500 or 0.01? Namely: Is it a problem of simulation conditions or summary? If it is a problem of simulation conditions, can this problem be solved?
0
This discussion has been closed.