Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

power loss

梦在深巷
梦在深巷 Contributor Level 1
edited May 2023 in General
image.png

Hello, I would like to ask whether the final simulation power loss value of the device thermal simulation system of Corey refers to the sum of the power loss of three power modules (6 SiC devices)? If the power loss of a single power module is to be obtained, is it only necessary to divide the loss value of the simulation result by 3? If you want to find the loss of a single SiC device, do you just divide the loss of the simulation result by 6?

This discussion has been closed.