Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

How to properly connect Tj and Tc for LTspice simulation of C6D10170H

LeoLuchetti
LeoLuchetti Contributor Level 1
edited August 2023 in Discrete Products

Hello, with other SiC Part models the Tj and or Tc pins need to be connected to a voltage source in order for the device to behave properly. How should the Temperature pins be connected for the model of C6D10170H?

I currently have just Pin 2 (anode) and the case (Cathode) connected to the circuit.

Thanks,

Leo

This discussion has been closed.