Troubleshooting SpeedVal Kit Half Bridge Motherboard
SNaidoo
Contributor Level 1
Good Day,
I am using the Wolfspeed Speedval Kit Half Bridge Motherboard with the Buck/Boost Filter Board. When I previously used the motherboard it worked fine but for our application, we desoldered the film capacitors and re-soldered 2 of them and the board is not working as before. The main issue I think is that when I apply the 12V, ~15 V shows up on the output. When I try to run the boost converter, I get an overcurrent error so I think that for some reason both FETs are being driven at the same time but I could be wrong. Could I get some help troubleshooting?
Thanks,
Surendra Naidoo
0
This discussion has been closed.