How to change the settings of the Dynamic switching test.
Hi
I have tried to use the Speedval Graphical User Interface (GUI) to perform the Dynamic switching test/ double-pulse test. The platform I use is TI Control Cards TMDSCNCD280039C on the motherboard MOD-MB-HB-0900V-40A. There are only parameters of "limits" in the settings, as shown in the figure. No matter what parameter I use, it just generates a 10us single pulse. Can anyone tell me how to change the settings of the double-pulse test, like turn-on time, and turn-off time? Thanks in advance.
0
This discussion has been closed.