Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

E3M0075120J2) Maximum value of the Is,pulse(diode pulse current)@Vgs=0V

JNagat
JNagat Contributor Level 1
edited March 2024 in Discrete Products

Could you tell me the maximum value of Is,pulse@Vgs=0V(not -4v)?

I can find the condition Vgs=-4v,but there are no 0v.

The Figure 9. describes conditions that are -4v,-2v,0v.

According to this diagram,Is maximum value of Is,pulse@Vgs=0V 80A?

Is it right?

pict.jpg

Regards,

JNagat

This discussion has been closed.