Meaning of data sheet
Davidgur
Contributor Level 1
In the data sheet relating to the above driver a value for Rgext is given as 5ohm and 2.5ohm, obviously incompatable with the claimed 14A drive. A further value for Rg is given as 0.3ohm and 0.4ohm.
How do these values corellate, if the external gate resistance is 5ohms how can the total gate resistance be 0.3ohms?
Tagged:
0