Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Speedval kit optimum PWM frequency

Options
mavern1
mavern1 Contributor Level 2
edited May 2024 in General

We have the speedvalkit platform with following configs

  1. MOD-PWR-MM-C3M0032120K
  2. 400uH Buck / Boost filter board

We plan to test a buck converter config from 800V to 400V DC. What is the desired PWM frequency the 400uH inductor has been optimized for peak efficiency . Our load is 12A current.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Urvi_Ahluwalia
    Urvi_Ahluwalia Wolfspeed Employee - Contributor Level 2
    Options

    Hello mavern1,

    The SpeedVal kit buck/boost boards are designed for general purpose evaluation. They were not optimized for a particular operating point or tested to identify the peak efficiency as a function of frequency. To find the frequency for peak efficiency, you will have to take some frequency vs efficiency measurements. Recommended frequency range is 20 to 100 kHz. I recommend referring to the synchronous "boost" application example in the SpeedVal Kit Half-Bridge Motherboard User Guide. 66 kHz is used for testing in that example. A few other guidelines on synchronous buck configuration are highlighted in Section 8.3 of the user guide.

    I hope this helps.

    Thanks!

    Urvi

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.