Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

C2M0045170D

MattM
MattM Contributor Level 1
edited April 2024 in Discrete Products

Hello Wolfspeed,

I am trying to design a Solid State Circuit Breaker, for low voltage AC, based on C2M0045170D(prototype). I am using Cadence Orcad X and I am not able to simulate a simple DC circuit .

When I run the simulation this error appear:

////////////////////////////////////////////////////////////////////////////////

X_U2.Ls2 N00328 X_U2.sv 2.603n Rser
-------------------------------$
ERROR(ORPSIM-16015): Unknown parameter.

////////////////////////////////////////////////////////////////////////////////

Looks like it doesn't recognize the serial resistance parameter.

When I try to remove Rser from the model then just to check if it works I get this error:

////////////////////////////////////////////////////////////////////////////////

ERROR(ORPSIM-16551): Floating point computation failed during Device/Model Load. Possible solutions: 1)Ensure that all device parameters are in valid range. 2)Try using .options LIMIT
Maths Exception Code:e06d7363 in device X_U2.xgmos.G2, Multiply(1.50525e+306, -4.99969e+06)
INTERNAL ERROR -- Maths Exception Code:e06d7363 in device X_U2.xgmos.G2, Multipl

////////////////////////////////////////////////////////////////////////////////

I have attached output file for the first and second simulation, the model downloaded from your website and a print screen of the circuit I used to test the simulation. I ve spent many hours trying fixing but with no luck. Please let me know if you can help me getting the model running for Cadence Orcad X (PSpice).

Best Regards

Matteo

This discussion has been closed.