Double Puls Test
Hello,
I would like to sweep different internal component sizes. Unfortunately it doesn't work with the Spice Directive. For example, if I sweep an Rgi there is only one curve even though according to the annotation step the component takes on different values.
But if I Ctrl+Right click on the component and enter different values of Rgi there then I get different courses of I(Rlow) current.
for example in this picture Rgi=2 Ohm
Rgi=10 Ohm
In this case the current has two different values at the beginning of the second pulse, why?
I would like to use the Spice directive as it is much easier to see different values at a glance. Can you please tell me what I'm doing wrong?
The same also applies to internal sizes such as Cag, Cug Clg or Cds, Cgd and Cgs.
I also liked to know what the difference is between G_Cgs and cgs.
Thanks in advance