LTspice E3M0075120J2 Temperature Rise Simulation
Hello Wolfspeed Team,
I'm working on a reference design and would like to promote your SiC MOSFET.
I'm trying to find the junction temperature rise from passing 5.67-A for 300-ms through E3M0075120J2 drain-to-source to make sure it stays below abs max. I know for a continuous DC temperature rise, I can use this equation, but seems unrealistic for 300-ms ON time.
I tried to simulate in LTspice and see 14°C rise for 300-ms, wanted to double check if I am simulating this correctly. I'm not confident because I tried to do a 60 second simulation and see 4000°C rise when it should not be greater than 199°C. Please take a look and would also like to know how the math works for calculating a transient Trise, I'll need to explain this in the reference design.
300 ms Trise Sim
60 sec Trise Sim
Best regards,
Tilden Chen
Solid State Relays | Applications Engineer