Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

C6D08065Q - Can you connect the N/C pins on the QFN package to a polygon to aid in heat dissipation?

Macker
Macker Contributor Level 1
edited July 2024 in Discrete Products

Hello. I am working on a passive rectifier PCB design using the C6D08065Q SiC diodes and I am wondering if connecting the N/C pins to a polygon would cause issues with the performance of the device. I am thinking that it would be beneficial to connect them to a large copper surface to help with heat dissipation. In addition, would it be safe to assume the same thermal management process as a SiC MOSFET in a similar package (vias to reverse of PCB then heatsink)? Thanks.

This discussion has been closed.