Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Change the driver board parameters

Emma
Emma Contributor Level 2
edited December 2024 in Module Products

Hello, I met some difficulties when selecting the type of drive board. I want to drive the CAS480M12HM3 half-bridge module, and I chose CGD1700HB3P-HM3, but I still need to change the drive voltage and drive resistance on the drive board to explore the influence of the drive loop parameters on the switching characteristics. How can I change the driving voltage and driving resistance?

Tagged:
This discussion has been closed.