Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

I want to find a product with FWD Diode in C3M0032120K sic-mosfet.

Advance
Advance Contributor Level 1
edited December 2024 in Discrete Products

I want to find a product with FWD Diode in C3M0032120K sic-mosfet.

But it doesn't come out well when I search it

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

    Advance
  • Advance
    Advance Contributor Level 1

    FWD Diode : C4D20120A

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hello Advance,

    Can you please clarify? All SiC MOSFETs have a parasitic body-diode from source to drain that can be used as a free-wheeling diode. It is however a regular diode with reverse-recovery. Please see the body-diode characteristics in the datasheet of C3M0032120K on pages 3 & 5.

    image.png

    Are you saying you're looking for a device with an additional diode in parallel with body-diode of C3M0032120K? Thanks!

    Advance
  • Advance
    Advance Contributor Level 1
    edited December 2024

    Thank you for your answer

    Could you look at the 8 page Fig.26 Clamped Inductive Switching Energy vs. Teature graph in the data sheet you sent me as a link?

    FWD = C3M0032120K

    FWD=C4D20120A

    There are two Sweeting Loss graphs like this.

    So I'm looking for a product where C4D20120A is connected as an additional diode to C3M0032120K like the graph of FWD = C4D20120A

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hello Advance,

    Thank you for the clarification. For Fig.26, C4D20120A is not connected as an "additional diode" to C3M0032120K. C4D20120A is only switch in the top position for Clamped Inductive Switching test and C3M0032120K is the DUT. Please find schematic below:

    image.png

    Wolfspeed doesn't have a product where an additional diode is placed in the same discrete package as the MOSFET die. However, it is possible to achieve this in a design using 2 separate (MOSFET and external diode) packages. Let me know if you have any other questions. Thank you!

    Advance
  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Advance
This discussion has been closed.