Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

SiC Schottky Diode Avalanche ability

MGU
MGU Contributor Level 1
edited December 2024 in Discrete Products

Hello,

Do SiC Schottky Diodes are avalanche proof ? I need an high voltage diode with no recovery, I will use C4D01120E in serial and I wonder if y need to equilibrate them (for example with TVS) or if they are avalanche proof.

Regards

Mathieu

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • SGhosh
    SGhosh Wolfspeed Employee - Contributor Level 1

    Yes, our diodes have avalanche capability. However it always depends on the energy during a certain time frame. TVS can also be used to protect the diodes and extra care needs to be taken of the power rating of the TVS.

    The performance data of our 20A part can be found in the following paper for Wolfspeed's diode. The 2A part has a smaller die and lower Avalanche energy.
    https://hal.science/hal-01373039v1/document

  • MGU
    MGU Contributor Level 1

    Thank you for your answer.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.