Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD300DA12E-XM3 Schematic / Pinout table

Options
DebugItAgain
DebugItAgain Contributor Level 1
edited May 2025 in Module Products

I have already reviewed the files below but was looking for something more.

https://www.wolfspeed.com/products/power/reference-designs/crd300da12e-xm3/?docid=cG9zdDoyMjM1NQ%3D%3D

I am looking for a lookup table that identifies the GPIO (like GPIO42) and the resulting sensor (Temperature Sensor X). The current schematic lists the peripherals and TI declares but given that TI's microcontroller can be remapped with X-Bar they could be any pin. It also appears that my original post never got posted, so here is another version.

Tagged:
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
    Hello,

    The schematic for the design can be downloaded from the link that you provided by navigating to the "Technical & Sales Documents" tab at the bottom of the page and selecting "CRD300DA12E-XM3 ALL Design Files", as pictured below. The "Controller" schematic shows all the pins that are connected to the LaunchPad (shown below); it can be used to identify any pin remapping.

    Thanks,

    Chris N.

This discussion has been closed.