Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Material for PCB Carrier in CRD600DA12E-XM3

Options
Duclair
Duclair Contributor Level 2
edited March 2025 in Module Products

Hello,

I would like to know what material was used to print/build the Gate drive PCB Carrier in CRD600DA12E-XM3. this is because there are different high voltage levels on the gate drivers and the carrier is in close proximity to each of them, is the carrier in plastic or is it painted metal of some sort?

Thanks.

Tagged:
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
    Hello Duclair,

    The gate driver carrier is made from powder-coated aluminum. It has been extensively tested to ensure no voltage proximity issues.

    Thanks,

    Chris N.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.