Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

NTC

Emma
Emma Contributor Level 2
edited April 2025 in General

When I was using CGD1700HB3P-HM3, I met some problems and hope to get your answers
The driver board has only NTC-P and NTC-N pairs of pins, but the input has two thermistor signals of NTC1 and NTC2. Which thermistor does this pair of pins correspond to?
Thank you very much. Looking forward to your reply

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4

    Hi Emma,

    NTC 1 and NTC 2 refer to the two nets of the one thermistor located inside the HM3 module.

    {3AD12132-026B-4A91-8F3B-3780872AC973}.png

    So the NTC-P and NTC-N differential pair on the gate driver represents the temperature from this one NTC.

    Best Regards,

    Austin C.

  • Emma
    Emma Contributor Level 2

    Thank you for your reply. Could you please clarify whether the thermistor refers to the junction temperature of the upper bridge arm or that of the lower bridge arm?

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4

    Hi Emma,

    Shamar summarized this well in the thread here.

    "Thank you for the question. We have recently released a thermal app note detailing the performance of the NTC and the implications of trying to measure the junction temperature using the NTC. It is much more thermally coupled with the case than it is the junction; so thermal events and interfaces taking place at the case such as cold plate flow rate and TIM quality, affect the sensitivity and accuracy of the NTC reading.

    You can find details of this in Section 4 of the App Note pasted below.

    PRD-08376: Thermal Characterization Methods and Applications | Wolfspeed"

    Thank you,

    Austin C.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.