Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

DC Short Circuit, DCLink Voltage Reversal, and Wolfspeed SiC MOSFET Body Diode Failure

Options
petercs
petercs Contributor Level 1

Do you recognize the problem with SiC MOSFET devices that they can fail from voltage reversal when the DC Link experiences a short circuit?

Please read the attached report.

Regards, Peter Cox-Smith

Cox-Smith Consultants Ltd, UK.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

    petercs
  • petercs
    petercs Contributor Level 1
    Options

    Thanks for looking at this issue. Can you please respond as I have more test results (10 units) that show failure of the body diode in Wolfspeed devices type CPM3 002112 0D ? I need to respond to my client next week and it would be valuable to include Wolfspeed's opinion.

    Regards, Peter

    Peter Cox-Smith, Cox-Smith Consultants Ltd.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hello petercs,

    Can you please confirm if you are using the bare die CPM3-1200-0021A or the discrete device C3M0021120D? It is unclear from your given part number. Thank you!

  • petercs
    petercs Contributor Level 1
    Options

    Hi TBhatia

    The tests were carried out using the TO247 discrete devices, although there is a plan to use the bare die in the final product.

    Peter

  • FrankWei
    FrankWei Wolfspeed Employee - Contributor Level 2
    Options

    Hi Peter,

    Thank you for your feedback. How many SiC MOSFET dies for each switch position in this traction inverter? the reverse current should be shared by the dies, right? and the current should go through two switches in serials. on the other hand, how many pcs of C3M0021120D are applied in the test? a single device C3M0021120D may not be able to survive from the current stress as mentioned in the test report. Thank you

    Regards,

    Frank Wei

  • petercs
    petercs Contributor Level 1
    Options

    Thanks Frank, I will reply at length later this week…Peter

    Peter Cox-Smith

    Cox-Smith Consultants Ltd

  • petercs
    petercs Contributor Level 1
    Options

    Hi Frank

    My client is an aerospace company designing an electrical system for an aircraft, including the main generator, which will have an AC to DC structure with a DC bus. Their concern is that a short circuit of the DC bus will cause voltage reversal, and stress, and failure to the body diodes. Failure is not acceptable in an aircraft. Their plan is to use WolfSpeed SiC MOSFETs in the converter and, as you suggest, there will be multi-chip switches; the components I have tested are single devices with the same characteristic as the individual chips. The client expects a wide range of characteristics of the individual chips and expect one device to carry most of the fault current. For example, I have tested 10 devices to failure. The voltage across the body diode at failure varied from 24V to 72V and the I squared t from 92.7 to 182.1.

    The design project must specify a protection circuit that can be qualified (to aerospace requirements) to always protect the body diodes, as there is no guarantee that multi-chip switches will always survive. In tests, I have included a damping circuit that prevents or limits the voltage reversal and all WolfSpeed devices survived the DC Short Circuit test with damping present. However all such circuits increase dissipation and/or weight, both undesirable in aircraft, but possibly essential.

    Alternatively we could accept the voltage reversal and add a low volts drop high pulse capacity diode to take the current and limit the voltage on the body diodes. The trick here is to find a suitable diode. Does WolfSpeed offer a suitable diode?

    I look forward to your further thoughts, Peter

    Peter Cox-Smith

    FrankWei
  • FrankWei
    FrankWei Wolfspeed Employee - Contributor Level 2
    Options

    Hi Peter,

    Thank you for your sharing! The diode will not carry current during normal operation. So a high current rating Si rectifier should be cost-effective. You may try this part. vs-80apf1-m3series.pdf or you can look for a diode with even higher current rating. Thanks

    Regards,

    Frank

  • petercs
    petercs Contributor Level 1
    Options

    Hi Frank

    I have done further tests. I used a high power protection diode in the test rig across the DC+ to DC- bus-bars adjacent to the MOSFET.

    When testing single MOSFETs, one part failed but at a higher DC+ voltage compared to the unprotected tests.

    Also I have tested a stack of 5 parallel MOSFETs to represent the arrangement inside a WolfSpeed module with multiple chips per switch. Only one stack tested so far, and the protection diode prevented any failure up to 750V, which was the maximum in the test plan. Without the protection diode, the stack failed at 495V; all the devices were damaged.

    We are discussing a rare event, when the DC bus is short-circuited and the DCLink capacitors are discharged. It is the inductance that creates an LCR circuit that oscillates and causes DC bus voltage reversal and damage to the body diodes. However, in aircraft systems, it will be important to specify what happens in the rare event, and how to guarantee protection of system converters if there is a DC bus.

    Obviously, I am working on a scheme to guarantee protection.

    Best Regards, Peter

    Peter Cox-Smith

    Cox-Smith Consultants Ltd

Sign In or Register to comment.