Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

speedfit tool

Options
lok
lok Contributor Level 1

why the three phase inverter simulation with c3m0075120K is avaliable in 1000W but in 1500W, it show a error like this. it is thought that the current limit is not the case to over the device limit, it seem unresonable.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Mhusain
    Mhusain Wolfspeed Employee - Contributor Level 3
    Options

    Hi Lok,

    Could you please provide the specific conditions under which you are running the inverter simulation? You can find this information on the summary page (the last page) of your simulation results. From there, either click on the printer icon to generate a PDF or the checkbox icon to download a .zip folder containing all the raw data, as illustrated in the image below. Having these details will greatly assist us in diagnosing the issue more effectively.

    Thank you!

Sign In or Register to comment.