Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Wolfspeed 300kw Inverter controller design

Options
GayanvDissanayake
GayanvDissanayake Contributor Level 1
edited February 24 in Module Products

Hello,

I would like to inquire whether you provide the Wolfspeed 300 kW inverter controller design PCBs in Altium format.

Best regards,

Gayan Dissanayake
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
    Hello Gayan Dissanayake,

    The source files were originally developed in OrCAD/Allegro. I attached Altium versions by converting the source files to Altium using the Altium Import Wizard. Please note that the Altium file conversion can introduce conversion artifacts that are not part of the original source files so please be aware of this risk when using these converted files. These files were converted to provide a starting point for interested users.

    Thanks,

    Chris N.

  • GayanvDissanayake
    GayanvDissanayake Contributor Level 1
    Options

    Thank you chris!!

    ChrisN
This discussion has been closed.