Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

error in speedfit

lok
lok Contributor Level 1

why there is 0 switching loss in sychronous switch

image.png

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • BlakeNelson
    BlakeNelson Wolfspeed Employee - Contributor Level 3

    Hi lok,

    In the buck converter, the synchronous MOSFET only has reverse recovery losses (as it does not conduct in forward mode). Many of our older generation 3 discrete device models are missing reverse recovery losses, and so when used in the synchronous position, they will report 0 W switching losses. Here is a comparison of one of our newest devices to an old one:

    image.png

    While these losses are small, we recognize that this is a model limitation. If you have specific parts that you need reverse recovery losses for, let us know and we will do our best to get you updated versions of those models.

    One other note, if the simulated reverse recovery losses are less than 0.005 W, they will also be reported as zero even though the losses are in the model.

    Thanks,
    Blake

    lok
  • lok
    lok Contributor Level 1

    thank you very much, i really need some parts that i need reverse recovery losses for, here are the lists:

    C3M0075120K

    E3M0160120K

    thank you for help!

Sign In or Register to comment.