Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

芯片 出流能力

wafer2026
wafer2026 Contributor Level 1

我想了解一下CPM4-0230-0255ES0A 芯片的能力。10并情况下的出流能力,以及是否还有新一代的芯片

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • simon_lin
    simon_lin Wolfspeed Employee - Contributor Level 1

    Hi Wafer2026,

    thanks for reaching out, 10pcs parallel CPM4-0230-0255ES0A 2300V 30mohm die current capacity, major depend on the module package and thermal performance, and just a reference for you, it is possible to have 300A-400A current rating for 10pcs CPM4-0230-0255ES0A parallel, And the new Generation die is in developing now, please you can check with our local sales.

Sign In or Register to comment.