Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Technical Inquiry: Significant discrepancy between datasheet IGSS Max and actual measurement

Alen
Alen Contributor Level 1

Hello Wolfspeed Team,

I am writing to seek clarification regarding the Gate-Source Leakage Current (IGSS) specification for the C2M0045170D.

The datasheet specifies a maximum IGSS of 600 nA at VGS = 20V and VDS = 0V. However, our customer’s bench test results show a significant deviation from this limit.

[Measurement Details]
Using a high-precision picoammeter at room temperature (25°C), we consistently measured a DC steady-state leakage current in the range of several pA (pico-amperes) at VGS = 20V.

Given the three-order-of-magnitude difference between the datasheet Max (nA) and the actual measurement (pA), the customer is concerned about whether these extremely low values are considered normal or if they might indicate a potential measurement error or an unexpected device characteristic. This is particularly important for them as they are evaluating this device for a series-parallel configuration and need to ensure long-term reliability and uniform behavior.

Could you please provide insight on the following points?

  1. Typical Value: What is the typical IGSS value at 25°C? Is the pA range expected for a healthy device under these conditions?
  2. Spec Definition & Guardband: Does the 600 nA limit represent a DC steady-state value, or does it include a testing guardband to account for equipment resolution, temperature variations, and high-volume production margins?
  3. Transient vs. Steady-state: Does the datasheet value account for any initial transient or displacement current during the gate-charging phase, or is it strictly for steady-state leakage?
  4. Measurement Methodology: Is there any specific test duration or specialized equipment setup recommended by Wolfspeed to correlate with the datasheet limits?

We would appreciate your expert guidance to help our customer move forward with confidence in their SiC-based design.

Best regards,

Atsushi Takayanagi
Field Application Engineer
Richardson RFPD

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 3

    Greetings:

    Our devices do have very low IDSS at 25C so what you measured is on the lowe end but not unreasonable when measuring with precision equipment. There is margin built into the specification to allow for product variability, temperature, as well as lower resolution fixtures, humidity, pcb contamination, etc. that can cause higher readings. The specification is a steady state measurement.

    Julius R

Sign In or Register to comment.