Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD60DD12N-GMB

Options
suhe
suhe Contributor Level 1
edited April 23 in Module Products

Hello!

I am very interested in the 60KWDAB.The official website describes the CRD60DD12N-GMB as follows: Through careful design, sufficient power transfer is achieved using only the leakage inductance of the high-frequency transformer, eliminating the need for bulky additional magnetic components. How is this achieved? Are there any limitations to the switching frequency of this design? Is it suitable for operation below 10kHz?
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
    Hello suhe,

    The CRD60DD12N-GMB was designed to operate with a high-switching frequency (100 kHz) and low leakage inductance (~8 uH) so that only the transformer leakage inductance would be necessary to successfully operate the dual active bridge (DAB). Through careful transformer design, this ~8 uH of leakage inductance can be manufactured. Operating below 10 kHz like you mentioned would not be feasible because you would lose zero voltage switching (ZVS) in most operating modes, the transformer current would increase significantly, and the transformer design would need to change dramatically. Many of the concepts of this reference design (e.g., power module routing, gate driver design, cold plate design, etc.) can be applied to other designs operating at different switching frequencies, but we recommend operating this reference design at its target switching frequency of 100 kHz. I provided a slide below that demonstrates some of the design tradeoffs with different switching frequencies.

    Thanks,

    Chris N.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5
    Options

    Hello suhe,

    I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

    Chris N.

This discussion has been closed.