Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

25 kW FM3 Three-Phase Inverter (CRD25DA12N-FMC) for motor control testing

Options
Ujala_MG
Ujala_MG Contributor Level 2
edited July 1 in Module Products

Hi!

We are currently using the Wolfspeed 25kW three-phase inverter for motor control testing and have encountered an issue with signal distortion—particularly at higher DC bus voltages.

Could you please let us know if you have experience testing this inverter for motor control applications? If so, we would greatly appreciate it if you could share details on how the inverter, power supply, and resolver were configured in your setup.

Additionally, if available, could you kindly share a photo or diagram of your test setup for reference?

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Employee - Contributor Level 4
    Options

    Hello Ujala_MG,

    We tested this inverter with a fixed R-L load in a recirculating setup. The test configuration is shown below, and more information can be found in Section 5.3 of the user guide. The setup used open-loop sine pulse-width modulation (SPWM) and was evaluated at various power levels. A resolver was not used during this testing.

    Thanks,

    Chris N.

  • Ujala_MG
    Ujala_MG Contributor Level 2
    Options

    Thank you for the information. Can you please let me know, what is the maximum power you have tested this inverter and at what DC link voltage and phase current?

  • ChrisN
    ChrisN Wolfspeed Employee - Contributor Level 4
    Options

    Hello Ujala_MG,

    We have tested this system to full power at 800 VDC and 30 Arms. I provided experimental efficiency sweeps at various switching frequencies below.

    Thanks,

    Chris N.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.