Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

NTC temperature sensing without gate driver cards

Options
NilsL
NilsL Contributor Level 1
edited September 2025 in Module Products

Hello,

I would be interested to know whether it is possible to measure the NTC temperature sensor output at the switches in case one does not use the gate driver card (the gate signal is provided with an external function generator). I am using MODMBHB0900V40A motherboard together with the CGD1700HB2MUNA gate driver and MODPWRMMC3M0045065K daughter card is being tested.

If it is possible what would be your recommendations on the setup for such a measurement?

Kind regards,

Nils

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 3
    Options

    Greetings Nils:

    The C3M0045065K package power daughter card does not come equipped with an NTC. Only the power daughter cards with SMD devices such as TOLL and TO-263-7L come with NTCs installed on the daughtercard.

    Gate driver cards such as the CGD1700HB2M-UNA do have provisions for measuring NTCs and converting the resistance to temperature and reporting it to the optional control card and graphical user interface (GUI).

    Julius R

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.