Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Requesting access to the CAN protocol library

Mahedi
Mahedi Contributor Level 1
edited September 2025 in General

Hello,

This is regarding the CAN GUI software that is used to communicate with the CRD25DA12N-FMC 25 kW Three-Phase Inverter. I wish to deploy this same functionality in a User Interface I am designing myself. Therefore, I am requesting access to the CAN protocol library with a list of all the CAN messages and the data description. If possible, a DBC file would be great.

Thank you and best regards,

Mohammed Mahedi Hasan

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5

    Hello Mahedi,

    I provided a picture of the default CAN message structure below.

    CRD25DA12N-FMC V1.0 - CAN Encoding.png

    Thanks,

    Chris N.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5

    Hello Mahedi,

    I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

    Chris N.

This discussion has been closed.