Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

3D model for the package GM3/GM4 with chip and NTC

Options
Quido_69
Quido_69 Contributor Level 1
edited October 2025 in Module Products

Hello,
for a project using power SiC MOSFET package GM3 and GM4. I need to design a liquid cooler optimized for the installation space. Is there any data available on the layout of semiconductor chips and NTC in the power module? The goal is to design a cooler so that the semiconductor chips are cooled as best as possible. The layout is important to me both for thermal simulations of the cooler's functionality and for designing the overall mechanical design of the power converter.

Thank you for your advice

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

    Quido_69
  • Quido_69
    Quido_69 Contributor Level 1
    Options

    I would need information about the chip and thermistor layout for power modules:

    CAB004M12GM4T, CAB5R0A23GM4T, CAB6R0A23GM4T

    Thank you for your advice

  • CFlack
    CFlack Wolfspeed Employee - Contributor Level 2
    Options

    Quido_69,

    This information is available and is only shared under NDA. I will contact you via your registered email and get you connected with the right people.

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5
    Options

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.