Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Wolfspeed's 60kW DAB unit-further discussion

Options
Vishnu
Vishnu Contributor Level 1
edited December 2025 in Module Products

Hi,

Chris has supported be for few concept on the DAB 60kW module for my earlier discussion (https://forum.wolfspeed.com/discussion/1108/wolfspeed-039-s-60kw-dab-unit#latest). Thank you for you support Chris.

We are trying to build or rework on the 60kW DAB module which you have provided with the schematic and other details. Need your few support on the gate driver which you designed.

  1. Did you see any false turn on immediately after the turn off SiC mosfet happens? Even if the Millers clamp circuit is activated via clamp pin of the gate drive IC.
  2. Do you have any results of Vgs and Id for any voltage ranges of input and output during turn off. I have observed the ZVS plots during turn on from https://www.wolfspeed.com/knowledge-center/article/maximize-efficiency-in-isolated-dc-converters-for-ev-fast-charging-systems/
  3. Kindly share the efficiency plot for different voltage levels you tested the prototype vs the power vs efficiency for gaining more confidence on our similar design.

Thanks and Regards,

Vishnu Sidharthan P
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
    ChrisN Wolfspeed Employee - Contributor Level 4
    Options

    Hello Vishnu,

    1. We did not observe this issue. Do you have waveforms demonstrating this behavior?
    2. We performed our initial testing at 800 Vin and 800 Vout, so our results are from those testing conditions. I provided some additional Vgs and transformer current plots below for your reference.
    3. As mentioned in (2), we performed our initial testing at 800 Vin and 800 Vout. We plan to collect data at additional operating points, but we do not have those plots to share yet.

    Thanks,

    Chris N.

  • ChrisN
    ChrisN Wolfspeed Employee - Contributor Level 4
    Options

    Hello Vishnu,

    I hope that answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

    Chris N.

This discussion has been closed.