Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Clarification on J7 High-Voltage Measurement Connections in XM3 Three-Phase Inverter

danusha
danusha Contributor Level 1
edited August 25 in Module Products

Dear Team,

I am referring to the XM3 Three-Phase Inverter Reference Design User Guide (PRD-06975), specifically the external high-voltage measurement connector J7 described in Section 2.2.2.

The user guide states that J7 provides three differential high-voltage measurement inputs through six pins:

  • Pin 1 – VA-P: Positive HV Measurement Input Phase A
  • Pin 2 – VA-M: Negative HV Measurement Input Phase A
  • Pin 3 – VB-P: Positive HV Measurement Input Phase B
  • Pin 4 – VB-M: Negative HV Measurement Input Phase B
  • Pin 5 – VC-P: Positive HV Measurement Input Phase C
  • Pin 6 – VC-M: Negative HV Measurement Input Phase C

The guide mentions that the -P and -M inputs are differential inputs and are stepped down by the voltage-sensing circuitry before being provided to the ADC.

I would like to clarify the practical power-stage connections for the three negative measurement terminals VA-M, VB-M, and VC-M.

For a standard three-phase inverter application:

  1. Are VA-P, VB-P, and VC-P intended to be connected directly to the respective A, B, and C inverter phase output terminals?
  2. Where should VA-M, VB-M, and VC-M be connected?
  3. Should all three -M terminals be connected to the mid-point of DC-link?
  4. Alternatively, are these inputs intended for line-to-line measurements, for example VA-P → Phase A and VA-M → Phase B?

If possible, could you please provide a wiring diagram or schematic showing the recommended physical connections of all six J7 terminals to the inverter?

Thank you.

~Anusha

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5

    Hello Anusha,

    The Vx-P and Vx-M connections are designed to be used for line-to-line (L-L) or line-to-neutral (L-N) measurements, depending on the end-system needs. The Vx-P and Vx-M connections both have input pre-scaling, so they can be attached to floating references or a common reference. For example, the schematic for the Phase A feedback circuit is below and shows the pre-scaling components. If performing line-to-neutral measurements, all the Vx-M connections should be attached to the common neutral.

    {E09379CD-EAAB-433C-99F1-B3B3C6CBDA86}.png

    These feedback measurements can be attached directly to the A, B, and C outputs or after filtering the outputs. Please note that the A, B, and C outputs produce square waves operating at the switching frequency, since there is no filtering on the outputs of the CRD300DA12E-XM3. The onboard voltage sensors do not have the bandwidth to directly capture the square wave outputs; the measurement circuits therefore include filtering to convert the square wave voltage outputs to sinusoidal measurements.

    Thanks,
    Chris N.

  • danusha
    danusha Contributor Level 1

    Thanks for clarification.

    ~Anusha D

This discussion has been closed.