Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Model behavior of body diode C3M0030170P

vhfrp94
vhfrp94 Contributor Level 1

Hello,

I am simulating a surge current event (negative to positive pole) in a half-bridge configuration using two C3M0030170P discrete SiC MOSFETs .During the surge event, both body diodes conduct simultaneously in the current path. The simulation diverges and fails to converge once the bus voltage exceeds a few tens of volts, regardless of the solver settings tried (Gear, Trapezoidal, modified TRAP) or timestep adjustments. My specific questions are:

  1. Is this a known convergence limitation of the C3M0030170P SPICE model under high forward current body diode conduction?
  2. The model documentation states that "variation of body diode turn-ON voltage with VGS is not modeled" — does this also affect the body diode I-V characteristics at high surge currents, making it unsuitable for this type of analysis?
  3. Is there a recommended model or simulation approach for evaluating body diode surge capability (I²t) in a half-bridge topology?

Thank you in advance.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Mhusain
    Mhusain Wolfspeed Employee - Contributor Level 3

    Hello,

    Thank you for your question.

    Wolfspeed discrete SPICE models are intended to simulate device behavior within the operating conditions specified in the datasheet, including the junction temperature range of -55°C to 175°C. During surge current events, particularly under destructive or near-destructive conditions, the junction temperature can rise beyond the modeled operating range. When the model is used outside its intended region, convergence issues and non-physical results may occur.

    For this reason, we do not recommend using the standard SPICE model to evaluate body diode surge capability (I²t) or destructive surge performance. Such analyses typically require more advanced electrothermal and failure-physics models that are beyond the scope of the behavioral electrical SPICE model.

    For surge current evaluation, we recommend relying on the datasheet surge current ratings and thermal impedance information. We hope this answers your question and provides clarification on the limitations of the SPICE model for this type of analysis. Please feel free to reach out if you have any other questions.

    Regards

Sign In or Register to comment.