Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD25BDA6512N-K

Raghu2189
Raghu2189 Contributor Level 1

Hi Wolfspeed team,

I have modified the CRD25BDA6512N-K 25 kW three-level T-type reference design for a 15–20 kW PMSM motor-drive application. Before we release it for PCB production, I would like to ask you to verify the modified schematic (attached: T-Type_Edited.pdf).

Operating conditions:

  • DC link: 750 V
  • Switching frequency: 45 kHz
  • Motor: 15 kW PMSM, rated 20 A rms, peak 35 A
  • Controller: PLECS RT Box 1 (replaces the TI controlCARD)

Changes from the original design:

  1. Replaced the HSEC8 controlCARD sockets (J13 HSEC8-160-01-L-DV-A-BL, J14 HSEC8-130-01-L-DV-A) with 3 × Samtec TSW-130-07-G-D pin headers. Pin assignments are unchanged (1–60 / 61–120 / 121–180).
  2. Changed all 5 gate-drive DC-DC converters from SN607 to MGJ2D151503SC (15 V in), to match the +15 V aux rail.
  3. Added terminal J3 (Würth 691137710002) for the 15 V aux input.
  4. Removed the Phase Protection sheet (relay K2, Q19, MOVs RV3/RV4, PHASE terminal J8). The motor connects directly to the inverter output.
  5. Renamed J7/J9 to J4/J5 (no electrical change).

Questions for production verification:

Q1. Can you confirm the modified schematic is electrically correct and suitable for production for a 15–20 kW PMSM drive?

Q2. Is MGJ2D151503SC a direct drop-in for SN607 gate driver power supplies with +15 V / −3 V still the recommended gate bias for C3M0032120K and C3M0025065K?

Q3. Without the grid-side LC filter, are there any concerns with driving a motor directly (dv/dt, common-mode current, motor cable length)? Do you recommend dv/dt or common-mode filtering?

Q4. Are the current sensor range, IL feedback scaling and Iocp over-current thresholds suitable for our motor peak current? Which components set the OCP trip level?

Q5. Does removing the output relay and MOVs create any protection or start-up issues?

Q6. For the PLECS RT Box interface (3.3 V PWM inputs, 0–3.3 V sense outputs over short wires), do you recommend any extra filtering, series resistors or ground pins?

Q7. Is the existing thermal design (heatsink, SiC device losses) adequate for 15–20 kW continuous motor-drive operation?

We are happy to share the Altium project files if that helps the review.

Thank you for your support.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

    Raghu2189
  • Raghu2189
    Raghu2189 Contributor Level 1

    Hi

    I am unable to upload modified schematic PDF, it is showing 403 bidden error. Can you help me out

  • Raghu2189
    Raghu2189 Contributor Level 1

    Dear Wolfspeed Support Team,

    I am currently working with the CRD25BDA6512N-K reference design and facing difficulties accessing the schematic component libraries in Altium Designer.

    The schematic components appear to be linked to Wolfspeed-specific libraries, which are not included in the available design files. As a result, I am unable to retrieve the corresponding schematic symbols.

    Could you please share the Altium Schematic Library (.SchLib) or Integrated Library (.IntLib) files associated with this reference design?

    Your support would be greatly appreciated.

    Thank you.

  • ChadF
    ChadF Wolfspeed Admin - Contributor Level 2

    Hello Raghi2189, 

    Thank you for the interest in our design and such a detailed question! This type of design review is something that we offer to our customers to aid in development of their systems. If there is a company associated with this ask, I will be able to assist you better. Also, as this is a public forum, there may be some other users who can help with your verification process. Finally, it seems you have not attached any files to this post, so if you could provide those that would greatly assist anyone who will be helping check your design. I have also attached a .zip file that contains the Altium Schematic Library. Please let me know if this works for you.

    Best regards,
    Chad F.

    Raghu2189
  • Raghu2189
    Raghu2189 Contributor Level 1

    Hi ChadF,

    Thanks for sharing the schlib file. Yes we are closely working with marine industry. We are developing proto for their usage if all the things goes fine. Then industry will scale the technology. I am unable to upload the file it is showing 403 error i think there is issue with server

  • ChadF
    ChadF Wolfspeed Admin - Contributor Level 2

    Hello Raghu2189,

    Are you trying to attach the raw files or did you compress them into a zip file? I am not certain on what Error 403 is, but the most common issue is trying to upload a file type that is not supported.

    Thank you,

    Chad F.

  • Raghu2189
    Raghu2189 Contributor Level 1

    I have tried both by adding Schematic pdf as well as zip file. It is showing 403 error.

  • Raghu2189
    Raghu2189 Contributor Level 1
    edited November 10
  • ChadF
    ChadF Wolfspeed Admin - Contributor Level 2

    Hello Raghu2189,

    I have attached the schematic file directly to this post so other users can access it without visiting an external site. Regarding your questions, I can assist with Q2. The remaining questions involve application-specific design considerations that are best addressed through direct engineering discussions. For the C3M0032120K and C3M0025065K devices, the recommended gate drive voltage is +15 V / -4 V, as specified in their respective datasheets available at the links above.

    Thank you for your interest in our design. I hope this information helps with your project.

    Best regards,
    Chad F.

  • Raghu2189
    Raghu2189 Contributor Level 1

    Hi Chad,

    Thank you for sharing the schematic and clarifying the recommended gate drive voltages.

    In the original CRD25BDA6512N-K reference design, the SN6507 with a Würth push-pull transformer generates a +15 V / −3 V gate driver supply.

    In our modified design, we have replaced the SN6507-based supply with the Murata MGJ2D151503SC isolated DC-DC converter to obtain the same +15 V / −3 V output.

    Since the recommended gate drive voltage for the C3M0032120K and C3M0025065K devices is +15 V / −4 V, could you please clarify the following?

    1. Is the +15 V / −3 V gate drive supply used in the original reference design still acceptable for these devices?
    2. Can we retain the Murata MGJ2D151503SC converter with +15 V / −3 V output, or would you recommend changing the negative gate bias to −4 V?
    3. Are there any additional design considerations when replacing the SN6507-based isolated gate driver supply with the Murata DC-DC converter?

    Your guidance would be greatly appreciated before we proceed with PCB fabrication.

    Thank you for your continued support.

    Best regards,
    Raghu

  • SudharsanC
    SudharsanC Wolfspeed Employee - Contributor Level 1

    Hi Raghu,

    1.The +15 V / −3 V gate driver supply is acceptable for the C3M0032120K and C3M0025065K devices. However, a +15 V / −4 V gate drive provides improved switching performance, including faster slew rate and higher dv/dt capability compared to +15 V / −3 V. The additional negative gate bias also increases immunity to false turn-on of the complementary switch during high-speed switching transients. (If the application operates at higher switching frequencies or has significant layout parasitics, EMI-induced noise and coupling effects can become more pronounced and may influence switching behavior: Pick a power supply with lower coupling capaciatance and higher CMTI)

    2. You can use the +15v and -3v Dual isolated power supplies from Murata it has slight variation in performance compared to +15 and -4V Vgs behavior (Look through datasheets Figs: 8-10 ) or you can look for Dual isolated power supplies from other manufacturer if you don't want to compromise on performance +15v and -4 variant (there are many which shares the same footprint).

    3.Look for power supplies which has higher isolation voltage (2.5 to 3 times greater than your application voltage level) and also pick a power supplies with lower coupling capacitance and with higher CMTI immunity.

    Thanks,

    Sudharsan C.

    Raghu2189
Sign In or Register to comment.