Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

number of devices (1200V/50A SiC MOSFET) for 100 KW inverter

woodshaker
woodshaker Contributor Level 1

What would be the rough estimate on the number of SiC MOSFETs needed to design this 100KW inverter? If we assume 400V bus and 1200V/50A SIC MOSFET. Can someone help on this?

Comments

  • AAnders
    AAnders Wolfspeed Admin - Contributor Level 4

    Hello,

    Thanks for your inquiry. The best way to get an initial estimate of the best device(s) for a given application is to use our SpeedFit tool. It allows you to model almost any topology in a matter of minutes by just providing a basic level of information about the operating conditions. Please take a look and let me know if you have any further questions. You can also check out this article on the subject.

  • woodshaker
    woodshaker Contributor Level 1

    I can use the the tool.

    I want to learn a systematic approach with formulas to derive the required number devices needed to achieve the power level. Can you help?

  • SiC_Power_Admin
    SiC_Power_Admin Wolfspeed Admin - Contributor Level 4

    Hi Woodshaker - sorry for the delay. Please give us a couple of more days to gather some resources that you can use.

  • YuequanHu
    YuequanHu Wolfspeed Employee - Contributor Level 2

    The bus voltage is 400V, why did you choose 1200V device? A quick Speedfit simulation using our 650V MOSFETs (3 or 4 in parallel) shows the following results, with 4 switches in parallel, you can get much lower junction temperature (only 83.8C).

    image.png image.png


  • SiC_Power_Admin
    SiC_Power_Admin Wolfspeed Admin - Contributor Level 4

    Hi Woodshaker - do you have a follow up question for the Wolfspeed team ?

This discussion has been closed.