Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

starting a DC-AC converter design

Wilder
Wilder Contributor Level 1

I am interested in building a DC-AC converter around a CASW300M17BM2 half bridge.

The CGD1200HBP-BM2 Companion Gate Driver is recommended, but it is only rated to 1200 V.

Is there a Gate Driver rated to 1700V so full advantage of of the 1700 V half bridge can be achieved?

Is there a recommended pwm controller that could provide input signals to develop a fixed voltage sinewave at a selectable fundamental frequency while switching the half bridge above 100 KHz?

Thank you for any advice!

This discussion has been closed.