Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Orientation of High and Low Side Gates

AnthonyH
AnthonyH Contributor Level 1

Our application for a CGD1200HB2P-BM2 requires us to fit into a confined space. With our existing design it would help if it was possible to modify the High and low side gates to orient the gate driver perpendicular to a CAS120M12BM2. So I was wondering if the Gates have a specific name that I could look for an adapter to achieve this or it almost looks like a re-solder of the gates could orient them correctly with the existing holes.

Tagged:
This discussion has been closed.