Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Request for the Details and Spice model of SiC power module (CAS325M12HM2 and TH-3231-R).

Luowei
Luowei Contributor Level 1
edited January 2023 in Module Products

I am using SiC power modules (CAS325M12HM2 and TH-3231-R) separately for an EV traction inverter.

I want to ask the following questions:

  1. Do you have the spice model for these two modules, especially CAS325M12HM2, that I can use in LTspice model or any solution to generate it with the other available spice models?
  2. Any cross-talk consideration for them? Now I am using -5 and +20V to drive. I am considering how low the negative gate voltage can go and the limitations for the power modules.
  3. Short-circuit consideration, how long the power module can handle the short circuit conditions and how much energy it can bear in a short period of time.

Feel free to ask any questions and give me any comments.

Best regards,

Luowei Wen

This discussion has been closed.