Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CAB016M12FM3 for drone application, humidity altitude, top hole, press-out fixturing

MNeuner
MNeuner Contributor Level 1
edited March 2023 in Module Products

Hello,

I wanted to ask if there is any technical information regarding the operating environment for the CAB016M12FM3? Of special interest would be the maximum altitude and the maximum humidity (eventhough it will be placed in a sealed housing).

Additionaly I wanted to ask why there is a hole on the top-side of the housing (big one next to the pins)?

Would it be possible to receive the CAD files for the Press-out fixturing? I have already found the Press-in fixturing in another post.

Thanks a lot in advance and best regards

Matthias Neuner

This discussion has been closed.