Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Maximum current for the evaluation board KIT-CRD-CIL12N-FMA

wybcityu
wybcityu Contributor Level 1
edited February 2023 in Module Products

Dear all


I'm trying to use 2x KIT-CRD-CIL12N-FMA to build a full bridge inverter. Are the PCB able to handle 30A current?


Thank you for your answer

Comments

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hello, thank you for your message. A member of our technical team is looking into your questions and we will respond shortly. 

  • BrettSparkman
    BrettSparkman Wolfspeed Employee - Contributor Level 2

    Hello wybcityu,


    Yes, the KIT-CRD-CIL12N-FMA PCB can support 30A based on copper widths, socket quantity, and module ampacity on the PCB in a standard benchtop environment.


    Thanks,

    Brett

  • BrettSparkman
    BrettSparkman Wolfspeed Employee - Contributor Level 2

    Hello wybcityu,


    One additional note, you will NOT be able to use the CVR that is provided with the kit for continuous operation, as it will be too much energy for the CVR. It can be replaced with an appropriately sized bolt, 2x washers, and a nut.


    Thanks,

    Brett

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.