Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Asking for the structure diagram of KIT-CRD-CIL12N-FMA

JunMing
JunMing Contributor Level 1
edited February 2023 in Module Products

Hi, Mr. / Ms.

I'm trying to build an inverter with the module CAB016M12FM3 and the driver board CGD1700HB2M-UNA. I think I need a platform to connect the module and the driver board. I have noticed that the platform KIT-CRD-CIL12N-FMA may be a good choice.

I'm asking for the structure diagram of KIT-CRD-CIL12N-FMA, which looks like the picture below. I can't find a structure diagram of KIT-CRD-CIL12N-FMA in its schematic provided by wolfspeed.

8cfd91d40676c7a78e606dbd6081a8a.png


In addition, do you think it's feasible to build an inverter with the platform KIT-CRD-CIL12N-FMA? I mean, if I buy three KIT-CRD-CIL12N-FMA platforms, and then connect their input connections(+V) to the positive pole of the power supply, and also connect their input connections(-V) to the negative pole of the power supply, and finally connect their midpoint connections to a three-phase load, will it work?

Please let me know if you have any questions, comments, or issues.

Thanks!

Comments

This discussion has been closed.