Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Gate resistor used in application note CPWR-AN28

Duclair
Duclair Contributor Level 2
edited May 2023 in Module Products

Hello,

In application note CPWR-AN28, peak voltage vs gate resistors are drawn in figure 25 and figure 26. I would like to know if the gate resistors as indicated on these graphs are only the external ones, or a combination of both internal and external gate resistors.

Thanks.

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4

    Hi Duclair,

    Do you mind to double-check the Application Note number or provide the title? I believe CPWR-AN28 refers to the mounting guide for the XM3 power module: https://assets.wolfspeed.com/uploads/2020/12/CPWR-AN28.pdf

    Best Regards,

    Austin C.

  • Duclair
    Duclair Contributor Level 2
    edited May 2023

    Hi. Sorry, the page title on windows explorer when I open the app note is CPWR-AN28, but I just noticed the right name of the file is rather : CPWR-AN45

  • AustinC
    AustinC Wolfspeed Admin - Contributor Level 4
    edited May 2023

    Hi Duclair,

    Thank you for specifying. The gate resistors listed in these plots refer to the external gate resistor (typically called RG-EXT) on the gate driver PCB only. These values also do not include the output resistance of the gate driver IC. For transparency, we utilized the Texas Instruments® UCC21710 gate driver IC for this testing.

    image.png

    Thanks,

    Austin C.

  • Duclair
    Duclair Contributor Level 2

    Ok, Thanks!

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.