Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

XM3 Inverter CAN Interface with PCAN device

Tom
Tom Contributor Level 1
edited October 2023 in Module Products

I'm trying to connect via CAN bus CRD300DA12E-XM3, three phase inverter unit, using a PCAN usb to CAN device. But I can't get it to connect. The drivers are installed and the PCAN-USB unit is working with another CAN device but not the Wolfspeed one. Does the XM3 come preinstalled with the correct firmware to interface with the CAN bus or do I have to flash the software initially? Is there a way to tell if the the software is installed correctly without the CAN bus working? Any LED blinking? Right now my unit has no LEDs blinking.

image.png image.png


image.png image.png


This discussion has been closed.