Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Dynamic thermal parameter for CAB006M12GM3

Tangwei
Tangwei Wolfspeed Employee - Contributor Level 2
edited January 2024 in Module Products

Hi Sir,

can we provide foster fourth-order thermal parameters of CAB006M12GM3 for customer, like below, thanks

image.png


Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Bdeboi
    Bdeboi Wolfspeed Employee - Contributor Level 3
    edited January 2024

    Hi Wei,

    Here are the parameters for a 3rd-order Foster network following the format below. This should be sufficient for the customer (I am having a small issue with the 4th-order). If they have to have a fourth order circuit, let me know and I'll get it fixed.

    R1 = 0.20759, R2 = 0.0028637, R3 = 0.022834

    C1 = 0.27484, C2 = 0.0012515, C3 = 0.033355

    image.png

    Here is a comparison between the CAB006M12GM3 Zth data and the 3rd order fit for the above parameters.

    image.png

    Thanks,

    Brian

  • Bdeboi
    Bdeboi Wolfspeed Employee - Contributor Level 3

    I was able to figure it out. Here is the 4th order.

    R1 = 0.0018372, R2 = 0.031065, R3 = 0.0082913, R4 = 0.19263

    C1 = 0.00084193, C2 = 0.12324, C3 = 0.016418, C4 = 0.35435

    image.png


    image.png


  • BlakeNelson
    BlakeNelson Wolfspeed Employee - Contributor Level 3

    Hi Tangwei,

    I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Blake

  • Tangwei
    Tangwei Wolfspeed Employee - Contributor Level 2

    thanks for great support!

This discussion has been closed.