Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Debugging Example Code for 300 kW XM3 Three-Phase Inverter [CRD300DA12E-XM3]

aja2234
aja2234 Contributor Level 1
edited May 2024 in General

Hey,

I'm running the example code for the 300 kW XM3 Three-Phase Inverter but I am receiving an error whenever I attempt to debug the code as per the instructions in the example code from the manual. I receive 2 error screens back to back as soon as debug the code which I have attached below. What can I do to resolve this issue?

Any help would be greatly appreciated. Thank you!

Error Screen 1:

image.png

Error Screen 2:
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
    aja2234
  • JHayes
    JHayes Wolfspeed Employee - Contributor Level 3

    Can you please verify the settings in the General Properties window matches the below and that the correct configuration is active?

    image.png
  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.