300 kW XM3 Three-Phase Inverter - CAN Connection Issue
Hello,
I'm working on connecting the Wolfspeed Inverter to my computer via the CAN line but am having difficulty setting it up. I am using the USB2CAN from Inno-Maker,
, and was able to set up the baud rate (100k) using an application from Inno-Maker. My issue now is that when I connect my computer to the Wolfspeed and open up the XM3 CAN Inverter Interface it shows me the error message that I have connection issues and that I should check the port config. I've provided the screenshot below of what I am seeing on my screen for both the command screen and CAN connection side.
What can I do to have my Wolfspeed send/receive data and connect to my USB2CAN adapter? What interface should I toggle to make this work?
Any help would be greatly appreciated.
XM3 CAN Command Screen Screenshot:
XM3 CAN Connection Screenshot: