Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Firmware file missiong when configure nxp control card for Evaluation Board

Puzhen_Yu
Puzhen_Yu Contributor Level 1
edited July 2024 in General

I bought half-bridge evaluation board and nxp control card. Now I want to configure my control card to give PWM signal. I go to the website (https://forum.wolfspeed.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.wolfspeed.com%2Fspeedval-kit-control-cards%2F) to download firmware and GUI. As the handbook discribed, there should be an file with form ".elf" but there is no files like this in the website. Could you please check if firmware of NXP is available?

image.png

Here is the screenshot of handbook for NXP control board configuration. To load the firmware, a file ".elf" is needed.

rolfhorn66
Tagged:
This discussion has been closed.